System Information Block (SIB) Transmission Setup

LTE TDD Signal Studio supports SIB transmission on DL-SCH with user defined SIB contents. This topic provides general information on system information blocks and an example setup. Refer to 3GPP TS 36.321 and 3GPP TS 36.331 for more details.

This topic contains the following sections:

System Information Transmission Overview

Example Setup

Assumptions:

Configuring the Signal Studio Software

Setting up Signal Studio (General)

  1. Start with the default setup for the N7625C Signal Studio software.

  2. Delete the existing carrier.

  3. Click Add Carrier and add Advanced LTE TDD Carrier.

  4. At the Downlink node, click the Predefined Config. button and select Full filled QPSK 10MHz (50RB).

  5. At the Carrier node, set Waveform Generation Length to 8 frames (80 ms) and Uplink Downlink Configuration to 1.

Setting up SIB1

  1. In the Channel Setup node, select DL-SCH1 and then change RNTI Type to SI-RNTI.

  2. Click Transmission Configuration Length and set to 8 frames (80 ms).

  3. Click Transmission Configuration to open the DL-SCH Tx Sequence window.

  4. Click button and Set all "State" to OFF.

  5. Click State to set the necessary state of the Subframe #5 of even number frame to on for the SIB transmission. (For this SIB1 transmission case, SIB1 transmission has to satisfy 3GPP section 5.2.1.2 of 36.331.)

    For this SIB Transmission example use the following settings:

    Sequence #

    Frame #:

    Subframe #

    State

    6

    0

    5

    on

    26

    2

    5

    on

    46

    4

    5

    on

    66

    6

    5

    on

  6. Click Column Preset and select MCS Index 0 to..., then enter 4 to satisfy Transmit Block Size ≤ Block Size 0.

  7. Click Column Preset and select Set all N_1A_PRB to 2 (default).

  8. Set each Subframe RV Index 0using the values below. This is for SIB1 transmission:

    Sequence #

    Frame #

    Subframe #

    RV Index 0 Value

    6

    0

    5

    ceiling (3/2*(SFN/2) modulo 4) modulo 4 = 0

    26

    2

    5

    2

    46

    4

    5

    3

    66

    6

    5

    1

    Refer to 3GPP section 5.3.1 36.321.

  9. Click OK to close DL-SCH Tx Sequence window.

  10. Click in the Data 0 cell to open the window and select User Defined Bits. Then enter your own generated SIB contents by importing or direct entry into the bit field. Append zero bit (“0”) to make data length equal to the TB size set in step 6. Click OK when finished.

Setting up SI1 (SIB2 and SIB3)

  1. In the Channel Setup node, select DL-SCH2.

  2. In the General Settings, set State to On for SI1 (SIB2 and SIB3) message transmission.

  3. In the General Settings, click the RNTI Type drop down and select SI-RNTI.

  4. Click Transmission Configuration Length and set to 8 frames (80 ms).

  5. In Transmissions Configuration to open the window.

  6. Click Column Preset and select Set all "State" to OFF.

  7. Set the required State of the Subframes to on for SI1 (for this example, SIB2 and SIB3) transmission.Click , State check box.

    For this example of the SI1 message transmission, it is assumed that the transmission on Sequence 15, Frame 1, Subframe #4 State = on. Transmission Sequence 15, Frame 1, Subframe #4 is just an example; you can select any subframe that satisfies the 3GPP standard. Refer to section 5.2.1.2 36.331.

  8. Select MCS Index 0 to satisfy the desired TB Transport Block Size ≤ setting Transport Block Size.  

    Example: where 30 bytes (240 bits) = TB Size

    1. Set MCS Index 0 to 8.

    2. Set N_1A_PRB to 2 (default).

    3. Verify that now displays 256.

  9. Set each Subframe RV Index 0.

    For this example:

    Sequence #12, Frame #1, Subframe #1, RV 0 = ceiling (3/2*(11 modulo 4)) modulo 4 = 1.

    Refer to 3GPP TS 36.321), section 5.3.1.

  10. Click OK to close he DL-SCH Tx Sequence window.

  11. Generate user-defined SIB contents (customer supplied) and insert the data into Data 0 on DL-SCH2 as User Defined Bits.

  12. Click OK to close the Data Source Selection window.